RampButton object
The RampButton object represents the intrinsic RampButton object. It is not a creatable object. RampButton objects are accessible through an Elements collection.
The RampButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback