PilotCtrlListSelector object

The PilotCtrlListSelector object represents the intrinsic PilotedControlListSelector object. It is not a creatable object. PilotCtrlListSelector objects are accessible through an Elements collection.
The PilotCtrlListSelector object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal