Panel object

The Panel object represents the intrinsic panel object. It is not a creatable object. Panel objects are accessible through an Elements collection.
The Panel object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal