PageUpButton object
The PageUpButton object represents the intrinsic PageUpButton object. It is not a creatable object. PageUpButton objects are accessible through an Elements collection.
The PageUpButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback