NavigationButton object

The NavigationButton object represents the intrinsic NavigationButton object. It is not a creatable object. NavigationButton objects are accessible through an Elements collection.
The NavigationButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal