MultistateIndicator object
The MultistateIndicator object represents the intrinsic MultistateIndicator object. It is not a creatable object. MultistateIndicator objects are accessible through an Elements collection.
The MultistateIndicator object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback