MoveUpButton object

The MoveUpButton object represents the intrinsic MoveUpButton object. It is not a creatable object. MoveUpButton objects are accessible through an Elements collection.
The MoveUpButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal