MoveRightButton object

The MoveRightButton object represents the intrinsic MoveRightButton object. It is not a creatable object. MoveRightButton objects are accessible through an Elements collection.
The MoveRightButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal