MoveDownButton object

The MoveDownButton object represents the intrinsic MoveDownButton object. It is not a creatable object. MoveDownButton objects are accessible through an Elements collection.
The MoveDownButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal