MaintainedPushButton object

The MaintainedPushButton object represents the intrinsic MaintainedPushButton object. It is not a creatable object. MaintainedPushButton objects are accessible through an Elements collection.
The MaintainedPushButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal