LocalMessageDisplay object

The LocalMessageDisplay object represents the intrinsic LocalMessageDisplay object. It is not a creatable object. LocalMessageDisplay objects are accessible through an Elements collection.
The LocalMessageDisplay object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal