ListIndicator object

The ListIndicator object represents the intrinsic ListIndicator object. It is not a creatable object. ListIndicator objects are accessible through an Elements collection.
The ListIndicator object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal