LinearGauge object
The LinearGauge object represents the intrinsic linear gauge object. It is not a
creatable object. LinearGauge objects are accessible through an Elements collection.
The LinearGauge object only exposes the properties and methods provided by the Element
object.
Properties
Methods
Provide Feedback