Line object
The Line object represents the intrinsic line object. It is not a creatable object.
Line objects are accessible through an Elements collection.
The object-specific properties for the Line object are merged with the Element object's properties. This extended object is what the user will see when directly accessing the object from VBA using the object's name.
Properties
Methods
Constants
Provide Feedback