LatchedPushButton object
The LatchedPushButton object represents the intrinsic LatchedPushButton object. It is not a creatable object. LatchedPushButton objects are accessible through an Elements collection.
The LatchedPushButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback