InterlockedPushButton object
The InterlockedPushButton object represents the intrinsic InterlockedPushButton object. It is not a creatable object. InterlockedPushButton objects are accessible through an Elements collection.
The InterlockedPushButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback