Image object
The Image object represents the intrinsic image object. It is not a creatable object. Image objects are accessible through an Elements collection.
The Image object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback