Gauge object

The Gauge object represents the intrinsic Gauge object. It is not a creatable object. Gauge objects are accessible through an Elements collection.
The Gauge object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal