EndButton object

The EndButton object represents the intrinsic EndButton object. It is not a creatable object. EndButton objects are accessible through an Elements collection.
The EndButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal