ControlListSelector object

The ControlListSelector object represents the intrinsic ControlListSelector object. It is not a creatable object. ControlListSelector objects are accessible through an Elements collection.
The ControlListSelector object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal