BarGraph object

The BarGraph object represents the intrinsic BarGraph object. It is not a creatable object. BarGraph objects are accessible through an Elements collection.
The BarGraph object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal