BackspaceButton object

The BackspaceButton object represents the intrinsic BackspaceButton object. It is not a creatable object. BackspaceButton objects are accessible through an Elements collection.
The BackspaceButton object only exposes the properties and methods provided by the Element object.
Properties
Methods
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal