Refine shapes (XY Plot)
Refine a shape by automatically adding points that are defined by the underlying data, to give added granularity to shape definition. The disadvantage of refining a shape is that it adds many more data points to the shape, which can make it difficult to drag points.
To refine a shape
- Right-click the plot surface and selectShape > Refine.
- Right-click the plot surface and selectShape > Editto view the added points.
Provide Feedback