Edit shapes (XY Plot)
You can edit the shape to manually change it or add points to it.
To edit a shape
- Right-click the plot surface and selectShape > Edit.
- Use the cursor to drag the points (square boxes) on the shape to change the shape.
- Right-click the plot surface and click one of the following:
- Add Point. Adds a point at the cursor's current location.
- Undo. Removes a point.
- Undo All. Removes all points that have been added using theAdd pointoption.
- Exit Edit. Exits edit mode.
Provide Feedback