Create shapes from existing traces (XY Plot)
When creating a shape from an existing trace, XY Plot
analyzes the underlying data and makes its best effort to mimic the trace data. The resulting shape will usually follow the shape of the data represented by the trace, but occasionally some data points may not be included in the shape. If this occurs, you can refine your shape
.To create a shape from an existing trace
- Right-click the plot surface and selectShape > New from Trace.
Provide Feedback