Set runtime properties and appearances as default (XY Plot)

XY Plot
general runtime properties and detailed runtime appearances and behaviors can be saved as default in the test run mode on the current computer.
The XY Plot
objects you create afterwards will inherit the default properties you configured earlier.
Specifically, these properties include:
  • General properties on the
    General
    tab of the
    XY Plot Properties
    dialog box
  • Detailed properties on the
    General
    tab of the
    Properties
    dialog box inside
    XY Plot Setup
    :
    • Time Period
    • Chart
    • Application
    • Live Data
    • Retrieval
    • Shape
  • Column settings including column width and which columns to show or hide
  • Overall look including layout and which toolbar buttons to show or hide using VBA
To set runtime properties and appearances as default
  • After you have configured the runtime properties and appearances in the test run mode, right-click anywhere within the chart, and then select
    Set as Default
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal