Chart page (XY Plot)

How do I open the Chart page (Properties dialog box)?
  1. In the
    Properties
    dialog box, click the
    General
    tab.
  2. Click
    Chart
    in the left pane.
Chart properties allow you to set the title, information that displays in tooltips, zoom, and other options that display in the current
XY Plot. The following properties are applied immediately to the current XY Plot.
The following options are available:
Property
Description
Title
The title to use. Select one of the following options:
  • Click the
    Use current trace label
    checkbox to change the title based on the trace that currently has focus. As different tags are selected, the title updates. The tag description displays along with the tag name.
  • Type a title for the chart in the field below the
    Use current trace label
    checkbox. This title will remain regardless of the trace that has focus.
You can set the title's font, style, size, and effects by clicking
Font
.
Margins
The amount of white space on the plot surface (in pixels).
Tooltips
Select the content of the tooltip from the following options:
  • Click the
    Show value
    checkbox to display the tag's value when hovering over a line in the chart.
  • Click the
    Show date and time
    checkbox to display the tag's time stamp data when hovering over a line in the chart.
  • Click the
    Show quality
    checkbox to display the tag's quality when hovering over a line in the chart.
  • Click the
    Show caption
    checkbox to display the tag's caption instead of the tag name when hovering over a line in the chart.
    Note:
    You must select
    Caption
    under
    Legend
    on the
    Traces
    tab for the caption to display in the tooltip.
Zoom and Pan
The display of the plot surface.
Select from the following options:
  • In the
    Zoom by
    box, type the percentage that you want to increase when using zooming or rubber band zooming to zoom in or out of a chart.
  • For the
    Display overlay panel
    checkbox, select whether to display a toolbar in the bottom right of the plot surface to increase, decrease, or reset the zoom.
  • For the
    Enable pan
    checkbox, select whether to allow panning the data by moving the mouse.
  • For the
    Pinch to zoom
    checkbox, select whether to allow using two fingers to zoom in or out of a canvas on a touch screen.
Automatic scaling
Determines the method used to automatically scale data based on the following:
  • From each individual trace.
    Uses the lowest and highest value for each trace in the chart. Values are separated into their own axis. For example, if you have a tag with values from 0-100, and another tag with values from 500-900, when you select the first tag, the Y-axis displays 0-100. When you select the second tag, the Y-axis displays a value of 500-900.
  • From all traces in the chart.
    Uses the lowest and highest values from all traces in the chart for the Y-axis. For example, if you have a tag with values from 0-100, and another tag with values from 500-900, the Y-axis would have a value of 0-900 to include values from both traces.
    This is useful, for example, for comparing two production lines side by side that have the same target. If you scaled them individually, both would look fine, but if you compared them side by side using the same scale, you might notice that the downtime on the second line was 20% higher than the first line.
    Note:
    Traces that have logarithmic mode enabled or have automatic scaling will be in a separate group and not combined with other traces in the chart.
Background
Determines the background color or image. Select from the following options:
  • To change the background color of the chart area, click the
    Color
    button beside
    Window Color
    and select a color.
  • To change the plot area's background color, click the
    Color
    button beside
    Canvas Color
    and select a color.
  • To change the plot area's background image, click the
    Browse
    button beside
    Canvas Image
    and select an image.
Cursors
Determines how the cursors display data when enabled.
Click the
Value differences
checkbox to display the difference between the value at the start of the cursor and the end of the cursor.
Trace layout
Displays each trace in its own grid or zone.
  • Click the
    Stack Y-axis
    checkbox to display each trace in a separate grid.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal