Statistics properties dialog box (XY Plot)
How do I open the
Statistics properties dialog box?
On the
Chart
tab of the Properties
dialog box, click Statistics
.If you use statistics, calculations are performed on the data sample set.
The following options are available:
Property | Description |
---|---|
Zones | The zones represent 1, 2, and 3 standard deviations from the mean for the sample. The following options are available:
Notes:
|
Mean line color | The color of the line that represents the mean of the samples. |
Provide Feedback