Zoom in or out (TrendPro)
The zoom feature allows you to zoom in on an area for detailed analysis.
To zoom in, do any of the following:
- Double-click an area of the plot surface you want to zoom in on.
- Press CTRL-plus on the keyboard.
- At the bottom right of the plot surface, click
.
- Scroll the mouse wheel up. Note that if you use the mouse wheel, it zooms relative to the location of the cursor on the plot surface.
- Put two fingers on the touch screen and move them apart to zoom in, ifPinch to zoomis enabled on theChartpage.
To zoom out, do any of the following:
- Shift-click an area of the plot surface you want to zoom out of.
- Press CTRL-minus on the keyboard.
- At the bottom right of the plot surface, click
.
- Scroll the mouse wheel down. Note that if you use the mouse wheel, it zooms relative to the location of the cursor on the plot surface.
- Put two fingers on the touch screen and move them together to zoom out, ifPinch to zoomis enabled on theChartpage.
Provide Feedback