View trace statistics (TrendPro)

Trend calculates statistics (including averages and time weighted averages) on the data being plotted on the graph. Statistics calculations are either performed on all the data, or across the time range represented by the two x-axis cursors.
The actual data used as the source for the statistics calculation displays in the
Trace Data
dialog box.
To view trace statistics
  1. On the
    TrendPro
    toolbar, click
    Statistics
    Trend Linked Icons PNG File Template.
  2. In the
    Calculate statistics
    list, select a time period to view.
    TIP:
    If you click
    X-Axis Cursors
    Trend Linked Icons PNG File Template on the
    TrendPro
    toolbar to turn on x-axis cursors, an option to calculate statistics for the time period defined by cursors displays in the list.
  3. Click one of the following:
    • Print Preview
      to preview the list before sending it to the printer.
    • Print
      to print the list.
    • Save
      to save the list to either a comma or tab delimited file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal