Trace Data dialog box (TrendPro)
How do I open the Trace
Data dialog box?
On the plot surface, right-click a trace and select
Trace Data
.You can view trace data for a specific period of time, and can organize it for printing. The following options are available:
Option | Description |
---|---|
Time period | Select a time period for which you want to display trace data. |
Narrow/ Wide/ Sparse Wide | Choose one of the following:
|
Print across pages | Select this check box to horizontally print trace data across multiple pages. |
TIP:
Consider the following:
- The displayed trace data respects the x-axis cursors. Data displays only for points within the cursors and the time period will show cursors.
- Tag names are truncated if name clashes exist (i.e., two tags are named the same but belong to different items).
- Time period tag values display a datetime, and discrete values display the associated true/false strings, if available.
You can click one of the following options:
- Print Previewto preview the list before sending it to the printer.
- Printto print the list.
- Saveto save the list to either a comma or tab delimited file.
Provide Feedback