Troubleshooting: Value bar is missing from trend chart

Problem
When you click a trend object at runtime, the value bar does not show.
Solution
The
Display Value Bar
setting on the
Display
tab determines whether a value bar shows on a trend chart. To make the value bar available at runtime, select the
Display Value Bar
check box.
The setting on the
Runtime
tab,
Allow Show/Hide Value Bar
, determines whether operators can toggle the value bar display at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal