Troubleshooting: Right-click menu does not work on the trend object
Problem
When you right-click a trend at runtime, the context menu does not work or is missing some options.
Solution
The context menu is set up on the
Runtime
tab in the Trend Properties
dialog box. If the context menu is not available or is missing options, it is because it was set up that way. To change the settings, open the Runtime
tab.Provide Feedback