Troubleshooting: Pen is missing from a trend chart
Problem
A pen does not show on the trend chart.
Possible solutions
Check the following:
- In thePen Attributesarea on thePenstab, make sure that theVisibleproperty isON.
- On thePenstab, make sure that the pen line color is not the same color as the chart's background color (set up on theDisplaytab).
- On thePenstab, if theData Point Connectionoption on theDisplaytab is set toShow Only Markers, make sure that the pen has a marker assigned.
- On theY-Axistab, check the chart range, as defined by theMinimum / Maximum Value Options. If the pen's data is all outside of the specified range, the pen's trend line draws at the top or bottom of the chart, where it may not be noticeable.
Provide Feedback