Troubleshooting: Grid lines are missing from a trend chart

Problem
A trend chart does not show horizontal, or vertical grid lines.
Cause
Several settings control the display of grid lines. Set up options for horizontal grid lines on the
Y-Axis
tab. Set up options for vertical grid lines on the
X-Axis
tab.
Solutions
On the
Y-Axis
, or
X-Axis
tab, check the following:
  • Verify that the
    Display Grid Lines
    check box is selected.
  • Verify that the number of major, or minor grid lines is set to a number greater than zero.
  • Verify that the grid color is not the same color as the chart background. Set up the chart background color on the
    Display
    tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal