Trend template

A trend template contains a set of trend settings. A template can be applied to all trends in an HMI server to create a consistent appearance. When you apply a template, the property settings selected for the template are applied to the current trend and will be evident on the runtime chart.
Use a trend template:
  • to apply consistent settings to multiple trend charts.
  • to build a set of different views for the same data.
  • as a quick way to return to a standard display after experimenting with options.
Operators can open the trend property tabs at runtime by right-clicking the control and then selecting
Properties
. You can also provide a button on the
FactoryTalk View
display that opens trend property tabs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal