Save pen changes at runtime
After you add one, or more pens to a trend chart at runtime, you can save the changes so that you can use those settings again later.
For example, an operator needs to look at pens 1, 2 and 3 at runtime, but those pens weren't configured with the project. Rather than add these pens every time, they close and reopen a trend, they want to be able to add the pens once, save them, and then the next time they run the trend, be able to load the pens without selecting them all again.
To save pen changes at runtime:
- On theTemplatetab of the TrendPropertiesdialog box, selectPens tab, and then in the right-hand pane, select thePenscheck box.
- ClickSave Template, and then type a name for the template.
- To use these settings, clickLoad Templateon theTemplatetab, select the name you gave this template, and then clickOK.TIP:If you create a trend template with tag placeholders in design mode, and then apply the template at runtime, the tag placeholders will not work. However, if you create a trend template with tag placeholders during runtime, the tag placeholders will work.
Provide Feedback