Print a trend chart display at runtime
To make printing a trend chart display available to operators at runtime, click
Allow Print
on the Runtime
tab. If the check box is cleared, operators cannot print the trend chart display.To print a trend chart display at runtime:
- Right-click the trend chart display and selectPrint Trend.
The report that prints includes the trend display, line legend, chart title, x-axis and y-axis legends, and current value legend.
Provide Feedback