Add an overlay to a trend and set it up

Use the
Overlays
tab to add an overlay to a trend.
To add an overlay to a trend and set it up:
  1. On the
    Overlays
    tab of the
    Trend Properties
    dialog box, click
    Add
    .
  2. In the
    Component Browser
    , select a snapshot name, and then click
    OK
    .
  3. Use the options in the
    Overlay Attributes
    spreadsheet to set up the anchor point, offset, initial visibility, and other details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal