Options in the Gradient Fill dialog box

The following table shows the options in the
Gradient Fill
dialog box.
Options
Descriptions
Colors
Move the slider to change the percentage of the start and end color.
Start color
Click the
Start color
box to choose the start color for the gradient fill.
End color
Click the
End color
box to choose the end color for the gradient fill.
Horizontal
Click
Horizontal
to make the color gradient in a horizontal direction.
Vertical
Click
Vertical
to make the color gradient in a vertical direction.
Diagonal Up
Click
Diagonal Up
to make the color gradient in a diagonal up direction.
Diagonal Down
Click
Diagonal Down
to make the color gradient in a diagonal down direction.
Styles
A linear gradient color is specified by two points, and a color (or different intensity of one color) at each point. Depending on the points' positions, there are four styles you can select.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal