Set up common properties of an object

Use the
Common
tab to set up the common properties for an object.
To set the common properties for an object:
  1. In the
    Graphics
    editor, right-click the object and then select
    Properties
    .
  2. In the
    Properties
    dialog box for the object, click
    Common
    .
Specify the common properties for the object.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal