Create a TrendPro object
Create a TrendPro object to show real-time or historical data from data sources:
FactoryTalk Alarms and Events, Live Data, FactoryTalk View SE data logs, FactoryTalk View SE DataLogPro, FactoryTalk Historian, FactoryTalk Historian Asset Framework,
.OSIsoft® PI Server™
, and FactoryTalk AssetCentreTo create a TrendPro object
- In the Toolbox, selectTrendPro.
- Drag the mouse to create a box approximately the size the trend chart is to be.
- On theGeneraltab, specify the general runtime options.
- On theCommontab, specify the common properties such as size and positions.
Provide Feedback