Add traces at design time (TrendPro)
At design time, you can add a trace as a tag or parameter to the trend.
For each trace on a TrendPro object, samples are plotted using a horizontal
x-axis representing time and a vertical y-axis representing the value.
TIP:
To show data from FactoryTalk View SE data logs, make sure the data log models are started. Otherwise, the trend will not show any value of your selected tags.
To trend historical data in
a FactoryTalk Historian
SE server, Asset Framework server, FactoryTalk Historian ME module, or PI Server
, you
need to install FactoryTalk Historian Connectivity
from the FactoryTalk View
installation package on the FactoryTalk View Studio or SE Client computer.All clients must use either the same computer name or the same IP address. If you add or delete a PI server, restart your FactoryTalk View Studio or FactoryTalk View SE Client to take effect.
To add traces to a trend at design time
- On theTracestab ofPropertiesdialog box, click
.
- To add the item as a tag:
- SelectTag.
- On theTag explorer, expand the tree and navigate to the folder for the data source.
- On theItemspane, select one or more tags or alarms.
- To add the item as a parameter:
- SelectParameterand then select a type.
- Type a format of#numbersuch as#1.
- ClickOK.
Provide Feedback