Define a client key
Use the Client Keys editor to define a client key in a client keys file. You can set up multiple client keys in one client keys file.
To define a client key:
- In, right-clickFactoryTalk View Studio, in the Explorer windows, navigation toLogic and ControlClient Keysand selectNew.
- In theClient Keyseditor, clickAdd.
- In theAdd Keydialog box, select a key from theKeylist.
- To create a key sequence, selectControl,Shiftor both, and then clickOK.
- In theClient Keyseditor, type a label for the client key.
- Click theBrowsebutton (...) beside thePress Action,Repeat Action, orRelease Actionfield, to open theCommand Wizardand choose a command or macro for the action.TIP:If a key action is to perform a task such as calling a macro, you should use the press or release action.
- When complete, clickOK.
- If prompted, provide a name for the client keys file.
Provide Feedback