Set up advanced data log path options
Use the
Advanced Configuration
dialog box to set up advanced data log path options. These options are associated with setting up secondary logging paths.To set up advanced data log path options:
- In theData Logs Modelseditor, in thePathstab, selectEnable Switchover to Secondary Path.
- Specify the secondary logging path, and then clickAdvanced.
- In theAdvanced Configurationdialog box, specifySwitchOverandSwitchBacktimes.
Provide Feedback