Start and stop data logging
You can use the context menu or command to start and stop data logging. When using the
DataLogOn
and DataLogOff
commands, you need to specify the data log model name. If you use an asterisk (*) with the DataLogOff
command, it turns logging of all models off.You can run this command from anywhere you can trigger the command, and the command is run on the HMI server side.
Provide Feedback