Example: On Event logging
You can set up an application so that it creates new log files at the end of a batch process or at the end of a shift.
For example, create a tag called
NextShift
. In the Data Log Models
editor, specify On Event
in the File Management
tab and type this tag as the expression. When the tag evaluates true a new data log file set is started to store information from the new shift.Provide Feedback