Example: Starting a new file at specified times
To start a new file every Wednesday at 2:00 am and every Friday at 2:00 pm, you would type the following start times:
- Wed 2:00
- Fri 14:00
You must type times and dates in the format indicated. You cannot use time and date formats specified by the Regional Settings of the Windows Control Panel.
Some information can be left unspecified. For example if you type
14:35
, it means start a new file every day at 14:35.If you type
:05
, it means start a new file every day and every hour at :05.Provide Feedback