Select servers to export strings from

This window only opens when you are exporting text strings from a network distributed application. It displays a list of all the HMI servers in the current network distributed application.
To select servers to export strings from:
  1. Select the check box beside the server or servers you intend to export strings from.
    To select all the servers, click
    Select All
    .
    To clear all the check boxes, which de-selects them, click
    Clear All
    .
  2. Click
    Next
    to continue.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal