Select an import operation
Use the
Import Operation
window of the String Import Export Wizard
to do the following:- Import strings for the language selected in theLanguage Configurationdialog box from one or more Unicode text files into the application.
- Import strings from an Excel spreadsheet for all the application's supported languages that are defined in the spreadsheet.
To select an import operation:
- ClickImport strings from a Unicode text file into <RFC1766 Name>to import strings from a Unicode text file into the application, for the language selected in the Language Configuration dialog box.
- ClickImport strings from an Excel spreadsheet into all application languages defined in the spreadsheetto import the strings from an Excel spreadsheet, for all of the application's languages that are defined in the spreadsheet.
Provide Feedback